Realtek Wireless LAN Driver

WinZIP self-installing ZIP file. Can also be unZIPped using PKUnZip 2.04g or equivalent.
This driver is needed to insure the proper operation of the Wireless LAN device in your computer.

Change Points

  1. Fixed: WLAN MAC address may change after a warm boot in Windows 7 (32bit/64bit). This issue may occur with Realtek RTL8723AE WLAN modules using driver version 2.00.0016 or earlier.

Installation Instructions

  1. Save this file to a convenient location such as the Windows Desktop
  2. Double-click the downloaded file icon.
  3. Answer the remaining prompts to complete the installation.
  4. Restart the computer.

Driver Version Verification

  1. Open Control Panel.
  2. Open Uninstall a program.
  3. Select Realtek WLAN Driver and verify that the driver version is V2.00.0020.

Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.