Clean Installation of Image
- Document ID: 4001315
- Posted Date: 2013-04-30
- Distribution: View Public Website
- Issue
Internet browser crashes, WiFi connection issues, and overall poor performance may be the result of a corrupt operating system.
- Resolution
A complete reinstallation of the operating system may be necessary. This procedure will allow for the system software to be completely reconfigured. This procedure requires a complete wipe of all data stored on the tablet.
- Procedure
This procedure will wipe all user data stored off of the tablet. Back up all data prior to starting.
- Download the special application which will enable Service Station to view the clean image. The file can be downloaded directly onto the tablet or transferred over. http://download.toshiba.com/PreImageUpdateApp5.apk
- Verify the tablet is plugged in, has an active internet connection, and change the display sleep to 30 minutes or higher.
- Install the downloaded Pre-Image Update Application.
- If a window window pops up titled Install Blocked as shown below select Settings > Security > Unknown sources and OK. Go back to the installed applications and install the Pre-Image Update Application.
5. Select Done when the application is installed.
6. Go to APPS, launch Service Station, and select Check for Updates.
7. Select, download, and install the latest Thrive System Image Update - PIU version (Thrive IMM76D.01.000072314 System Image Update - PIU version at the time of publication of this document.)
8. Select Update System after the update has downloaded.
9. After the system updates go to Settings > Backup & Reset > Factory data reset > Reset tablet > Erase everything.
10. After the tablet resets and restarts the software has been completely reinstalled.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.