Toshiba Video Player

Package
WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
Description
This is a TOSHIBA Video Player update.

Change Points

  1. Fixed: DVD Playback will stop after showing the logo when playing some DVD titles.
  2. Fixed: Application hangs when maximized if the taskbar is positioned on the top of the Desktop.
  3. Fixed: Cannot auto change 3D resolution on some titles.
  4. Improved the color setting function.

Install Instructions

  1. Save the downloaded file to the Windows Desktop.
  2. Save all work in progress and close open applications.
  3. On the Windows Desktop, double-click the downloaded file to start the installation.
  4. Click Start when the Toshiba Archive Extractor window is displayed.
  5. Click Yes to continue if a User Account Control window is displayed.
  6. Follow the displayed instructions to complete the install.

Version Verification

  1. Launch TOSHIBA Video Player.
  2. Press the ? button on the top right corner of the video window.
  3. Verify the version is 5.3.18.82.

Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.