ACPI Flash BIOS version 1.40 for Satellite W35Dt (PSD24x)
- File: sd24v140.exe
- Version: 1.40
- Posted Date: 2013-12-19
- Release Date: 2013-11-04
- Other Versions
-
Release Date: Version: 2014-06-06 1.50 2013-12-19 1.30 2013-12-19 1.20 2013-12-19 1.10
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
- For CD-ROM BIOS updates in Windows 8 or 8.1 models: (1) Shut down the system while pressing the SHIFT key to completely power off. (2) Press the F12 Key while powering on to access the Boot Menu. (3) Select the device with the BIOS CD-ROM and press the ENTER key. (4) Type BIOS then press Enter.
- Note: The BIOS Launcher "CD_ROM Installation" option may not automatically proceed to burn the CD-ROM in Windows 8 or 8.1. If this occurs navigate to the directory named after the BIOS filename in the root directory of the C-Drive (ex. C:\skgjv130), and manually burn the CD-ROM from the disc image (ISO) file.
- For CD-ROM BIOS updates in Windows 7 models: (1) Boot from the BIOS CD-ROM. (2) Type BIOS at the C:\ prompt then press Enter.
- For all updates: The BIOS update will force the computer to shut down or restart. Please make sure to save all work in progress before starting BIOS updates.
- Power on the computer if it is off.
- While the "TOSHIBA" logo is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Release Notes
Change History
- Version 1.40 - 2013-11-04
- Fixed: Keyboard battery does not charge, and battery "Not Present" error.
- Updated: Pad Embedded Controller (EC) to version 1.10 and the Docking EC to version 1.30.
- Modified: USB device boot behavior.
- Updated: Samsung memory SPD table.
- Updated: "RTC battery is low" message with GUI interface.
- Updated: Pad EC.
- Modified: ASL code to support Windows 8.1.
- Fixed: Power button issues.
- Fixed: OSD Keyboard cannot input a User Password in tablet mode .
- Updated: Pad & Dock Embedded Controller (EC).
- Initial production BIOS release for these models.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.