DTS Studio Sound
- File: OS2014126A_TC00...
- Version: 1.1.45.0
- Posted Date: 2014-04-01
- Release Date: 2014-04-01
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
- This driver provides audio enhancements for your computer.
Prior to installing this driver, please install Realtek Audio Driver V6.0.1.7195 or higher.
Change Points
- When installed in conjunction with Realtek Audio Driver V6.0.1.7195 or higher the following issue is resolved:
- DTS function is disabled when repeatedly going into standby or hibernation while playing content.
Installation Instructions
- Save this file to a convenient location such as the Windows Desktop
- Save all work in progress and close open applications.
- From the Windows Desktop, run the downloaded file to start the installation.
- If a User Account Control or Open File message is displayed, press Continue.
- Press the Start button at the Toshiba Archive Extractor window.
- Follow the displayed instructions to complete the install.
Driver Version Verification
- Open Control Panel.
- Select Programs and Features.
- Find DTS Studio Sound Driver.
- Verify that the driver version is 1.1.45.0.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.