WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
This is the WinDVD BD for Toshiba version 8 patch for the following versions:
  • 8.0 DXVA B20.107
  • 8.0 DXVA B20.153
  • 8.0 DXVA B20.174
  • 8.0 DXVA B20.185
Please check your current version using the version verification procedure below before performing the upgrade.

Change Points

  1. This patch fixes a problem where noise is heard while playing the Avatar Blu-ray Disc.

Install Instructions

  1. Save the downloaded file to the Windows Desktop.
  2. Save all work in progress and close open applications.
  3. On the Windows Desktop, double-click the downloaded file to start the installation.
  4. Click Start on the Toshiba Archive Extractor window.
  5. Click Yes to continue if a User Account Control window is displayed.
  6. Click OK when the installation completes.
  7. Restart the computer.

Version Verification

  1. Start WinDVD BD for TOSHIBA.
  2. Right-click, and choose Setup from the pop-up menu.
  3. Click the Information tab of the Setup dialog box.
  4. Click the Driver tab.
  5. The version number is shown just below Version.

Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.