ACPI Flash BIOS version 1.80 for Satellite L640D/L645D (PSK0QU)



File: sk0qv180.exe




Version: 1.80
 
Posted Date: 2011-03-10

 

Release Date: 2011-02-18

 

Other Versions

 

Package
WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
Description

Release Notes

  • After the update completes, the computer will automatically shut down or restart.
  • Power on the computer if it is off.
  • While the "Toshiba" LOGO is displayed, press the F2 function key to start BIOS Setup.
  • Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
  • Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.

Change History

    Version 1.80 - 2011-02-18
    • Updated the ATI (Park XT S3) Video BIOS to support new Hynix and Samsung Video RAM dies. Note: This is not a recommended update for PSK0QU-xxxxxx model owners as this change applies to future production that will be sold outside the U.S. or Latin America.
    Version 1.70 - 2010-09-09
    • Realtek 8191SE and 8188CE ASPM set to L0's and L1. Also set the bridge 0xE4 bit 23.
    • Updated reference code for SB820 A13 (Update_CIMX_SB_1100)
    • Added a warning message to the Fast Boot screen if a boot device is not found.
    • Limited the DDR3-1333Mhz DRAM speed to 1066Mhz.
    • Fixed: User password shows "password fail" if HWsetup sets the keypad "/"key as part of the password.
    Version 1.50 - 2010-05-14
    • Fixed: Fails to restart in Windows XP when installing Toshiba Power Saver and the Hotkey Utility.
    • Fixed: The computer wakes up automatically from Stand By (S3) in Windows XP.
    • Fixed: An incorrect battery serial number is reported to the OS.
    • Fixed: The LCD brightness level increases after pressing native hotkeys in Windows XP.
    • Removed ALPS TouchPad support - no longer used.
    • Fixed: When Core Multi-Processing is disabled in BIOS Setup, the splash screen logo will change from "Vision" to "BC."
    • Changed the HDD default password mode to User only.
    • Fixed: When F2+PowerButton is pressed, fast boot mode is intermittently not disabled.
    • Fixed: SmartDE (HDD Encryption SW) system hang issue.
    • Fixed: Triple core CPUs will "setvariable" several times during POST.
    • Fixed: HDD head parking sound can be heard when shutting down in XP or DOS.
    • Fixed: Blu-ray playback delay - Blu-ray ODD equipped models only.
    Version 1.40 - 2010-04-16
    • Initial production BIOS for the Satellite L640D/L645D PSK0QU model.
Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.