WinDVD BD for Toshiba

WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
This is the WinDVD BD for Toshiba upgrade for the following versions:
Please check your current version using the version verification procedure below before performing the upgrade. If your WinDVD BD version does not match any of the versions above, this update is not for your computer.

Change Points

Playback issues were fixed for the following titles.
  1. Die Fantastischen Vier - Live in 3D
  2. Battle for the Planet of the Apes - Japanese Title
  3. The Sorcerer's Apprentice - Japanese Title

Install Instructions

  1. Save the downloaded file to the Windows Desktop.
  2. Save all work in progress and close open applications.
  3. On the Windows Desktop, double-click the downloaded file to start the installation.
  4. Click Start on the Toshiba Archive Extractor window.
  5. Click Yes to continue if a User Account Control window is displayed.
  6. Click OK after the update module has installed successfully.
  7. Restart the computer.

Version Verification

  1. Start WinDVD BD for TOSHIBA.
    1. Click Start, All Programs, Corel, then Corel WinDVD BD.
  2. Right-click, and choose Setup from the pop-up menu.
  3. Click the Information tab of the Setup dialog box.
  4. The version number is shown just below Version.

Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.