ACPI Flash BIOS version 8.00 for Satellite Pro 490/490X
- File: 2490tv80.exe
- Version: 8.00
- Posted Date: 2000-02-12
- Release Date: 2000-02-07
- Other Versions
-
Release Date: Version: 2001-07-27 7.50 2001-07-27 6.30
Satellite Pro 490CDT |
Satellite Pro 490XCDT |
- Package
- WinZIP Self-extracting ZIP file creates bootable BIOS update installation diskette when run under Windows. Also self-extracts under MS-DOS or can be unZIPped using WinZip, PKUnZip, or equivalent.
- Description
Change History
-
Version 8.00 ???02-07-2000
- A change was made to support Windows 2000.
- A problem was corrected that when running Windows 98, with a SCSI card used in the PCMCIA slot, and the computer set to "Standby", the computer would hang when shut down.
- Corrected a problem where having the "USB Legecy=Enabled" set in the BIOS, and entering some keys on a Japanese USB keyboard, was impossible.
- Corrected a problem of installing a driver from the FDD. Installing a driver was impossible when a new device was detected during Windows 98 installation.
- This version was re-packaged / re-posted on Feb 20, 2003.
- Corrected a problem where the machine didn't boot when turning it on after cold docking the machine with the Enhanced Port Replicator III.
- Corrected a problem where the system would hang during a resume if the system was docked with an Enhanced Port Replicator III under WinNT5.0.
- Corrected a problem where the system could intermittently hang when trying to exit HyperTerm under Win98.
- Corrected an issue which could cause the display to hang in the Corel Draw 5.0 application.
- Corrected to eliminate the problem where, under Windows 98, the display state would be left with only a blinking cursor after a Display auto-off event when the Toshiba Windows 98 Utilities are installed.
- Corrected to pass the unreported memory test (HCT 7.6)
- Adds ACPI functionality for Windows 98
- Corrected a problem which, in Windows NT, prevented the Display Auto Off and HDD Off from working correctly.
- Corrected a problem, which in Windows 98 (Bld1723.4 and greater), could cause system hangs after resume. This failure would occur after resuming a system which had been put into standby mode with the USB Legacy Enabled.
- A modification has been made to allow the system to boot from a TEAC CD-ROM drive.
- Initial Production BIOS for these models
Version 7.50 ???08-19-1998
Version 6.30 ???08-13-1998
Version 7.40 ???08-10-1998
Version 7.20 ???07-13-1998
Version 6.20 ???06-11-1998
Version 6.10 ???04-27-1990
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.