Using the Addonics PCMCIA CD-ROM with the Recovery CD for the 3XXX series
- Document ID: 98050351
- Posted Date: 1999-08-09
- Last Updated: 1999-08-09
- Distribution: View Public Website
- Applicable Models
Portege 3010CT Portege 3015CT Portege 3020CT Portege 3025CT
- Issue
- Using the Addonics PCMCIA CD-ROM with the Recovery CD for the 3XXX series
- Procedure
- Make a copy of the recovery boot diskette and put the original away in a safe place.
- Boot the laptop holding F8 to get the startup menu.
- Choose COMMAND PROMPT ONLY.
- Insert the copy of the recovery boot diskette.
- At the prompt type "A:" and then ENTER.
- At the "A" prompt type CD MICRO and then ENTER.
- At the new prompt type EDIT CONFIG.SYS
- Place an REM (space) in front of DEVICEHIGH=a:\micro\arccdens.sys
- Place the cursor at the end of this same line and press the ENTER key (this will create a new line)
- On the new line, type device=a:\micro\pcmi80cl.sys /port=300 /mem=CE00
- Press the ENTER key, (this will start another line)
- Type device=a:\micro\statpcdm.sys /d:arccd01
- Hit ALT+F, then hit the letter "X"
- When prompted to save hit the letter "Y"
- Remove the recovery floppy from the "A" drive.
- Insert the CD-ROM manufacture installation diskette
- (NOTE: Contact Addonics Technical Support for this step if needed)
Copy pcmi80cl.sys and statpcdm.sys to the root of the "C" drive . - Remove the CD-ROM driver diskette, and re-insert the recovery boot diskette.
- Type "A:" then press the ENTER key.
- Type copy c:\pcmi80cl.sys a:\micro then press the ENTER key.
- Type copy c:\statpcdm.sys a:\micro then press the ENTER key.
- Reboot the laptop with the recovery boot diskette in the drive.
- When prompted to make a CD-ROM choice. choose option 3.
- Recovery will now run, At the welcome screen follow the instructions.
The EDIT command can be found on the companion diskette if not already present on the system.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.