Satellite 1800: Installing the modem driver for Windows XP (yellow exclamation point in Device Manager)
- Document ID: 98070343
- Posted Date: 2001-11-26
- Last Updated: 2006-06-27
- Distribution: View Public Website
- Applicable Models
Satellite 1800-S203 Satellite 1800-S253 Satellite 1805-S203 Satellite 1805-S253 Satellite 1805-S273
- Issue
The modem in the Satellite 1800/1805 is not working, after the installation of Windows XP. Control Panel / Device Manager shows a yellow exclamation point next to the entry for the modem.- Resolution
Follow this procedure to install the device driver for the modem:1. Open Device Manager, from the Windows Control Panel, by clicking Start, then Control Panel, System, Hardware, Device Manager.
2. Double-click the Modems (or Other Devices) entry.
3. If there is an entry for "Toshiba Soft Modem AMR", followed by a yellow exclamation point, continue with this procedure. Otherwise, click Cancel button, close Control Panel, and search for a different solution to your modem problem.
4. Double-click the entry for "Toshiba Soft Modem AMR".
5. Click the Drivers tab.
6. Click the Update Drivers button.
7. Select "Install from a list or specific location (Advanced)". Click Next.
8. Select "Don't search. I will choose the driver to install." Click Next.
9. In the Found New Hardware Wizard window, select Modems. Click Next.
10. In the Install New Modem / Manufacturer list, select "Toshiba" and from the Modem list select "TOSHIBA Soft Modem AMR (TOSHIBA)" or "TOSHIBA Soft Modem AMR (Microsoft). Click Next.
Windows will now install the driver for the modem in the Satellite 1800/1805.
Once the installation is complete, return to Device Manager to verify that there is no longer a yellow exclamation point next to the entry for "Toshiba Soft Modem AMR".
- km/wa
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.