Autorun Fails Intermittently With Toshiba CDRW & DVD/CDRW Combo Drives
- Document ID: 98070528
- Posted Date: 2002-04-02
- Last Updated: 2002-04-02
- Distribution: View Public Website
- Applicable Models
Satellite 1905-S277 Satellite 1905-S278
- Issue
If a CD-ROM media with autorun file is inserted to the above drives, the autorun feature will normally not work.
Press the drive button to remove the CD, wait about 10 seconds and re-insert the CD into the drive. The autorun feature will start 4 out of 5 times.
The intermittent failure issue happens more often on the combo DVD/CD-RW drive than the CD-RW drive.
- Toshiba DVD/CD-RW SD-R2102
- Toshiba CD-RW SR-C8002
- Resolution
Disabling the Norton Auto Protect switch from the Task Tray will fix the Autorun failures.
By default, Norton Auto Protect switch is Enabled.
To disable Norton Auto Protect, toggle the Norton switch ON or OFF from the task tray without shutting down the machine.- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.