ACPI Flash BIOS version 1.70 for Satellite P200/P205 (PSPB0U)
- File: sp200v170.exe
- Version: 1.70
- Posted Date: 2007-09-13
- Release Date: 2007-09-06
- Other Versions
-
Release Date: Version: 2007-08-09 1.50 2007-05-25 1.40 2007-04-26 1.30 2007-04-10 1.10
- Package
- WinZIP self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included README file for details.
- Description
Change History
- Version 1.70 - 2007-09-06
- Changed the logo.
- Added a workaround in the BIOS code to prevent an automatic password (spontaneous password) issue.
- Added: Nvidia NVIF TV mode support function due to a new driver requirement.
- Corrected: A password may be automatically set during a DOS BIOS update from V1.60 to V1.70.
- A change was made to in the EC BIOS code to prevent a PWR_OK signal glitch when turning off the computer in battery mode.
- Updated the BIOS code to show the total memory capacity in the BIOS setup menu.
- A change was made to the Embedded Controller (EC) volume control algorithm to improve volume control stability.
- The CPU microcode was updated.
- A workaround was added for a LG panel LP171WP4-TLB1 garbage issue.
- A modification was made to solve an issue where the "Fn sticky key" function was still enabled after waking from S3 or a Fn+F1 (lock).
- Added a function to turn off the backlight and delay 800ms to turn on the backlight if the panel is a LP171WP4-TLB1.
- A workaround was implemented to correct a Realtek 8101E LAN Driver 186.1103.2006 issue that caused the computer to automatically wake from hibernation.
- Initial production BIOS for these models.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.