Intel Display Driver for Windows Vista V7.14.10.1272
- File: driver_display_...
- Version: 7.14.10.1272
- Posted Date: 2007-12-14
- Release Date: 2007-12-07
- Package
- WinZip Self-extracting ZIP file. Can also be extracted with PKUnZip 2.04g or equivalent.
- Description
-
Corrected issues from version 7.14.10.1217
- The display changes to a lower resolution (800x600 pixels) after closing the lid to put the computer in a sleep state, then resuming in Windows Vista.
Driver Install Instructions
- On the Windows Desktop, double-click the downloaded file to start the installation.
- Click OK, then click Unzip.
- Click OK, then click Continue if a User Account Control window is displayed.
- Answer the remaining prompts to complete the driver installation.
- Restart the computer.
(1) Save the file to the Windows Desktop:
(2) Install the new driver:
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.