Toshiba Value Added Package for Windows Vista
- File: util_tvap_os200...
- Version: 1.1.7
- Posted Date: 2008-01-11
- Release Date: 2007-12-14
- Other Versions
-
Release Date: Version: 2009-12-16 1.2.33
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using PKUnZip 2.04g or equivalent.
- Description
- The Toshiba Value Added Package includes Toshiba Common Modules as well as Power Saver,
Accessibility, Fnesse, Toshiba Utilites.
Special note: This application is for computers using the InterVideo WinDVD player.
Install Instructions
- Save the file to the Windows Desktop.
- Install the Toshiba Value Added Package (TVAP).
- Save all work in progress, and close all open applications.
- On the Windows Desktop, double-click the downloaded file to start the installation.
- Click OK, then click Unzip.
- Click OK, then click Continue if a User Account Control window is displayed.
- Click Next after the computer reboots, then click Next again.
- Answer the remaining prompts to complete the installation.
- Reboot the computer after the installation completes.
TVAP V1.1.7 Installation Confirmation:
- From the Start Menu, click Control Panel.
- Click Programs, then click Programs and Features.
- Confirm the version of "TOSHIBA Value Added Package" is 1.1.7.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.