Toshiba Value Added Package for Windows Vista
- File: util_tvap_os200...
- Version: 1.1.7
- Posted Date: 2008-01-11
- Release Date: 2007-12-14
- Other Versions
-
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using PKUnZip 2.04g or equivalent.
- Description
- The Toshiba Value Added Package includes Toshiba Common Modules as well as Power Saver,
Accessibility, Fnesse, Toshiba Utilites.
Special note for Portege M400 computer owners: Update the TOSHIBA RAID utility on your computer to V1.4.1.1 or higher before running this "Toshiba Value Added Package" update.
TOSHIBA RAID Utility V1.4.1.1 can be downloaded from the Portege M400 PC Support Downloads page at this link.
You may also search for a newer version of this audio driver on Toshiba's Service and Support site, at support.toshiba.com.
For general assistance with downloads, see Support Bulletin 98081213 Obtaining downloads and support docs from the Toshiba Support website.
Install Instructions
- Save the file to the Windows Desktop.
- Install the Toshiba Value Added Package (TVAP).
- Save all work in progress, and close all open applications.
- On the Windows Desktop, double-click the downloaded file to start the installation.
- Click OK, then click Unzip.
- Click OK, then click Continue if a User Account Control window is displayed.
- Click Next after the computer reboots, then click Next again.
- Answer the remaining prompts to complete the installation.
TVAP V1.1.7 Installation Confirmation:
- From the Start Menu, click Control Panel.
- Click Programs, then click Programs and Features.
- Confirm the version of "TOSHIBA Value Added Package" is 1.1.7.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.