Toshiba Software Modem for Windows Vista (64-bit)
- File: driver_modem_to...
- Version: 2.1.87
- Posted Date: 2008-05-02
- Release Date: 2008-04-24
- Other Versions
-
Release Date: Version: 2008-03-26 SM2187ALS03 2009-09-02 2.2.97 2009-09-02 2.2.97 2007-09-19 2.1.77
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using PKUnZip 2.04g or equivalent.
- Description
- This is the Toshiba Software Modem driver for the Windows Vista 64-bit operating system.
Versions
- 2.1.87
Change Points
Changes were made to correct the following:- The Modem does not work on PCs using the TOSHIBA Software Modem with Windows Vista 64-bit and 4G RAM.
Driver Update Instructions
- Save the file to a convenient location such as the Windows Desktop.
- Save open files and close all open applications
- Remove the old driver:
- From Control Panel select Programs, then "Programs and Features"
- Select "TOSHIBA Software Modem."
- Click "Uninstall/Change" button and then confirm the removal by clicking Yes.
- Click "Yes" to restart the computer.
- Install the new driver:
- Double-click the downloaded file to begin the update.
- Follow the instructions to complete the update.
Toshiba Software Modem version verification
- Run "Device Manager." ( Start -> Control Panel -> System and Maintenance -> Device Manager )
- Double-click Modems.
- Double-click Toshiba Software Modem.
- Click the Driver tab.
- Confirm the driver version.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.