ACPI Flash BIOS version 5.60 for Satellite A100 (PSAA5U/PSAAKU)
- File: sa100a5v560.exe
- Version: 5.60
- Posted Date: 2008-10-22
- Release Date: 2008-10-10
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Change History
- Version 5.60 - 2008-10-10
- Disabled C3 to correct a no boot/intermittent hang with T2060 CPUs.
- Corrected: A BIOS password may be set automatically (spontaneously) by the computer.
- Corrected: The internal keyboard repeat speed can not be changed.
- Added: "Battery critical wake up" at 5% enable/disable function.
- Added: When the battery capacity <= 5% in DC mode during BIOS Setup, the Critical Battery Wakeup item will be enabled to wake the computer from standby.
- Corrected: Intermittent boot failures with T2060 CPUs caused by EC resets of the south bridge.
- Added: ATIF interface for ATI systems where the TV Type is consistent with the BIOS Setup Menu.
- Updated: Execute Disable (XD) function.
- Updated: Virtualization Technology function.
- Modified: A 3-second pre-charge will be performed before switching to quick charge mode.
- The pre-charge current was changed from 128mA to 256mA to correct rare occurrences of battery recharge failures.
- Note: BIOS V5.00 (and higher) can be used with Windows Vista and XP. BIOS V1.30 (and lower) can not be used for Windows Vista. Once you update to V5.00 (or higher), you cannot revert to V1.30 (or lower).
- Modified the HDD password CMOS area so it is clear if a HDD password does not exist.
- Vista Capable PC updates; Note: This BIOS supports Windows Vista and XP.
- Added: BIOS interface to fix production test tool issues.
- Updated: Micro code for Yonah Celeron M430/440/450 CPUs.
- Added: BIOS & EC support for LP154W01-TLE4, LP154W01-TLD4, LP154W01-TLH1 display panels
- Modified: Force loading of CMOS defaults when the BIOS is updated.
- Corrected: Japanese words in the BIOS Setup Menu help file.
- Corrected an issue where F1 and F2 error messages were displayed after restarting, on computers without TOSHIBA Power Saver.
- Corrected an anomaly where the computer shuts down, instead of transitioning from standby to hibernation properly.
- A change was made to the maximum and minimum shared VRAM sizes.
- Corrected an intermittent auto shutdown issue that occurred when the F2 hotkey was continually depressed before the LCD turned on.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.