ACPI Flash BIOS version 4.70 for Satellite P100/P105
- File: sp100v470.exe
- Version: 4.70
- Posted Date: 2009-03-04
- Release Date: 2009-02-18
- Other Versions
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Change History
- Version 4.70 - 2009-02-18
- Per new spec., the BIOS password is copied to EEPROM and the CMOS and EEPROM password values are compared during POST. If the values are different, the BIOS will copy the EEPROM value to CMOS.
- Improved: VGA Fan did not work properly.
- Added support for flash part MX29LV008CT.
- Corrected a BIOS password(s) automatic deletion issue.
- Corrected: Windows Vista does not recognize the battery immediately when the AC Adapter is plugged-in.
- Added 64-bit OS support.
- 3D graphics performance was improved when combined with nVIDIA graphics driver update version 7.15.11.5666.
- Corrected: Power switch intermittently needs to be pressed for more than 5 seconds before the computer powers on.
- A workaround was implemented to prevent a password from automatically being set by the computer.
- A BIOS update was applied due to Intel's request.
- Note: BIOS versions 3.30 and later support Windows Vista and XP.
- Changes were made to support Windows Vista. This BIOS supports both Windows Vista, and Windows XP.
- Added the PCI_MEMORY_OPTIMIZATION option for 4GB of memory.
- Updated the NVIDIA G73M VBIOS.
- Added a ACPI 3.0 backlight control method for Windows Vista.
- Added a CX20549 Pin configuration setting for Windows Vista.
- Removed NVIDIA GPU WMI for Windows Vista.
- Corrected an issue where letters were dropped while typing normally after the MSN search toolbar was installed.
- Update the VBIOS to improve graphics performance of the nVIDIA G71M-Ultra chip.
- Corrected: When a password is set, If F12 is pressed continuously while booting, the computer will start up without a password.
- Changed the default setup menu language to be based on the part number.
- Added the Merom 6F1 CPU MCU RID 012.
- Corrected a Merom 6F1 CPU string display error.
- Changed the DMI BIOS release date year setting from 2 digits to 4 digits.
- Removed the EC & VBIOS version from the setup menu info page.
- Corrected a DMI BIOS version error.
- Updated the VBIOS for the nVidia G71M, G71M-Ultra, G72M-V, and G73M graphics.
- Added the Int15 function to set the TV out and the setup language from EEPROM.
- Modified VGA detection to apply different VGA fan tables.
- Modified the password feature to clear the user password when the supervisor password is cleared.
- Added Calistoga BSU 1.03.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.