Toshiba HDD/SSD Alert



File: util_HDD_alert_...




Version: 3.0.0.1
 
Posted Date: 2009-06-23

 

Release Date: 2009-06-23

 

Other Versions

 

Package
WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
Description

HDD SSD ALERT

The TOSHIBA HDD/SSD Alert includes wizard functions to monitor the Disk Drive operating status and execute system backup. TOSHIBA HDD/SSD Alert has the following features:

  • Notification of disk drive status - Disk Drive has the SMART Predict Failure function which monitors the Disk Drive operating status. TOSHIBA HDD/SSD Alert supervises this status and if a failure is predicted, it shows the alert message and recommends you backup data in the drive.
    NOTE: Please note that SSD technology only allows for a certain number of rewrite cycles. During the lifetime of your computer you may be required to exchange the SSD.
  • Disk Drive status - You can check current drive status by opening the TOSHIBA HDD/SSD Alert form the start menu.
  • System backup wizard function - This function executes Windows Complete PC backup.
    NOTE: For more information about the Windows Complete PC backup and recovery, please refer to "Backup and Recovery Center" in the "Maintenance" section.

IMPORTANT:

(1) The SMART function of disk drive can not predict all failures. It is recommended that you periodically back-up your Disk Drive data to external media.
(2) The administrator privilege is required for setup.
(3) The administrator privilege is required for system backup.
(4) The HDD recovery area does not get backed up. It is recommended that you create recovery discs using TOSHIBA Recovery Media Creator.
(5) Windows Complete PC backup does not support backup of a second drive. The data of a second drive can be backed up by copying to an external drive etc. using Windows Explorer.

*Windows Complete PC backup is supported only by Windows7,Windows Vista Ultimate/Enterprise/Business. You may backup using a 3rd party's backup software if you use WindowsXP,Windows Vista Home premium or Home Basic.

To open the HDD/SSD Alert current status:

  1. Click the Start menu.
  2. Enter "HDD" into the search field.
  3. Click "HDD SSD Alert" in the search results.
  4. The HDD SSD Alert status will open and display the current status of your drive.

For complete information on the HDD SSD Alert, click the "Help" button after entering the HDD SSD Alert.


***NOTE*** This software package is part of the pre-installed software for the applicable products.
Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.