ACPI Flash BIOS version 2.10 for Satellite A305 (PSAGCU/PSAG8U)
- File: sagcv210.exe
- Version: 2.10
- Posted Date: 2009-11-06
- Release Date: 2009-11-05
- Other Versions
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Change History
- Version 2.10 - 2009-11-05
- Updated the Computrace OPROM 887.
- Changed the "Intel Virtualization Technology" default setting from Disabled to Enabled.
- Modified the critical battery wake up prevent value from 2% to 5%.
- Modified the battery low blinks, battery LED value from 2% to 10%.
- Modified the S3 Critical Battery wake up value from 5% to 8%.
- Updated: SLP2.1 for Windows 7.
- Added support for the Win7 Container ID function.
- Added: Check for 25W CPUs.
- Updated: PPM1.04 reference code.
- Updated: MRC2.8 reference code.
- Added support for the TVAP "Alarm power on" functions for the Win7 tool.
- Added support for the 2009 DMI 32 and DMI 64 utilities.
- The CMOS Year/Month/Date default setting is changed to 2009/07/01 after a RTC battery failure.
- Enabled SSP to fix a TS-L633C/TOYF 6029B0026509 "not found" issue.
- Modified: English "Yes" and "No" to French in the French BIOS Setup.
- Modified: BIOS Setup and F12 menu strings from "USB Memory" to "USB".
- Added a 25W CPU AC Adaptor total power setting value.
- Updated: MRC2.6 to fix a GL40 Rev A1 hang issue.
- Fixed: When the Illumination LED setting in BIOS Setup is changed from on to off and BIOS Setup is exited without saving, the Illumination LEDs are off.
- Fixed: Hitachi Panther-B HDD is not detected.
- Updated: ICH9M Ref 2.0 code.
- Updated: Cantiga R2.5 code.
- Updated: MRC2.5 code for the GL40 Chipset.
- Modified: FreeDOS CD file for BIOS upgrades.
- Added support for the Silego clock generator.
- Updated: Cantiga 2.3 reference code.
- Fixed: WinXP set to SATA Controller Mode "Compatibility" then Primary IDE Channel setting to "PIO mode."
- Save CRID value to CMOS bank1 4Ah for tool checking.
- Removed unused CPU microcode.
- Fixed: Need to input the supervisor password to open HWSetup if BIOS setup is entered first.
- Fixed: Boot priority is set to the default setting after restarting when "compatibility" mode is selected.
- Fixed: Setting the password in HWSetup with "Fn+0" can not be identified in SCU.
- Updated MRC v2.30 for Intel Cantiga A1 stepping.
- Fixed: The Celeron processor can not control the speed in the XP TPS application.
- Updated Insyde Flash Windows v3.54 to support the UAC function check.
- Added CRID Cantiga A1: 09h.
- Fixed: When the system boots to a PXE-Linux Server, file downloads take a longer time.
- Added support for T3200 and T3400 CPUs.
- Fixed: Can't display the Core Multi-Processing item after disabling the Core Multi-Processing function.
- Fixed: Can't boot from the USB FDD after setting defaults in BIOS without connecting a USB FDD.
- Updated Intel MRC to version 2.0.
- Fixed: GL40 + 4G RAM no Audio issue.
- Added the Tj85/Tj90/Tj100 thermal table.
- Fixed WINXP S3 resume fail when system used GL40 + Intel WLAN.
- Corrected a problem with finishing the initial Windows setup.
- Added Robson item in the SCU.
- Updated the thermal table to support Merom CPUs.
- Updated Turbo Memory 1.7 kernel code.
- Added 1067A CPU microcode.
- Corrected: 8GB RAM in 64-bit Operating Systems system runs very slow.
- Updated MRC code to v1.5.
- Modified the GL40 SSID.
- Added the Insyde H2O logo.
- Modified DVM and maximum graphics memory size.
- Corrected: After a S4/Resume, the "resuming" progress bar is not displayed in Windows XP.
- Corrected: Compatibility mode will blue screen (A5h).
- Changed the Hotkey function from "LED On/Off" to "Mute On/Off."
- Corrected: During Media Player operation, the sound is interrupted when Hotkey #1 "Illumination Led On/Off" is pressed in European models.
- First production BIOS for Satellite A300/A305 PSAG8U models.
- Corrected: Internal Keyboard repeat speed can not be changed.
- Initial Production BIOS for Satellite A300/A305 models (PSAGCU).
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.