Synaptics Touch Pad Driver for Windows 7 (32/64)



File: driver_touchpad...




Version: 14.0.11.0
 
Posted Date: 2010-02-02

 

Release Date: 2010-02-02

 

Other Versions
Release Date:Version:
2012-02-2915.3.39.0

 

Package
WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
Description
The Touch Pad driver is required for proper operation of your Touch Pad.

Change Point

  1. Fixed: When using the touchpad scrolling function, the scrolling regions are too thin to use.
    • Note that the driver version is the same as the existing version (14.0.11.0), but the registry information has been changed to make the scrolling regions larger.

Driver installation

  1. Save the file to the Windows Desktop.
  2. Close all open applications and save all work in progress.
  3. On the Windows Desktop, double-click the downloaded file to start the installation.

Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.