Realtek Wireless LAN Driver for Windows 7 (32/64)

Package
WinZIP self-installing ZIP file. Can also be unZIPped using PKUnZip 2.04g or equivalent.
Description
This driver is for computers configured with the Realtek RTL8191SE Wireless LAN adapter. Before downloading this driver package, please verify the type of Wireless LAN adapter that is in your computer.
  • Run Device Manager.
  • Double-click Network Adapters, and verify that Realtek RTL8191SE Wireless LAN 802.11n PCI-E NIC is listed
  • .
If a Wireless LAN adapter other than the Realtek RTL8191SE is in your computer, this driver should not be downloaded.


Changes From Previous Version

  1. Fixed: The Wireless LAN card stops working and can not be detected by the system.


Installation Instructions

  1. Save this file to a convenient location such as the Windows Desktop
  2. Save all work in progress and close open applications.
  3. Double-click the downloaded file icon to start the installation.
  4. Click OK, Unzip then OK again.
  5. Click Yes if a User Account Control window is displayed.
  6. Click Next, then click Install.
  7. Click Finish.
  8. Restart the computer.


Version Verification

  1. Run Device Manager.
  2. Double-click Network Adapters, then double-click Realtek RTL8191SE Wireless LAN 802.11n PCI-E NIC.
  3. Select the Driver tab and verify that the driver version is 2007.1.1002.2009.


Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.