ACPI Flash BIOS version 2.90 Tecra A11/M11 PTSE0U/E1U/E3U, PTME0U/E1U/E3U
- File: tse0v290.exe
- Version: 2.90
- Posted Date: 2010-12-15
- Release Date: 2010-12-14
- Other Versions
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Change History
- Version 2.90 - 2010-12-14
- Improved battery management.
- Improved DeployCenter 5.5 recovery speed.
- Added support for the McAfee Endpoint Encryption eToken.
- Added support for the Paragon Backup & Recovery Suite.
- Improved docker feature behavior - addresses missing Undock Start Menu option in Windows 7.
- Added support for 2011 non-Windows models.
- Implemented the INTEL specification for the Intel 5 Series Chipset to improve stability.
- Implemented the INTEL specification for the Intel Core i7/i5/i3 Mobile Processor Series to improve stability.
- Improved USB device recognition.
- Fixed: Audio skips when Eco mode is on during DVD video playback in Windows Vista.
- EC-1.90: Modified: BIOS BootBlock does not update when BIOS is updated.
- Fixed: The system may hang-up when an Expresscard is connected.
- Provided an interface in BIOS Setup to select the NumLock status while booting up.
- Fixed: May take long time to boot if a USB device (Black berry 9700) is connected to the system.
- Fixed: Booting a PCDOS GhostCD (v11.0.2) will cause a "Boot Failure" message.
- Optimized the condition when booting from a USB stick - addresses a USB stick boot issue when "USB-FDD Legacy Emulation" is enabled.
- Improved: Symantec Ghost V11.5.1 hangs if the system boots from an ODD, or USB memory.
- Improved: PXE boot menu can not be retrieved from the PXE server.
- Improved: No log-on screen on an external monitor after standby and hibernation.
- Implemented the Intel specification for the Intel Core i5/i3 Mobile Processor Series to improve stability.
- Improved boot time.
- Improved: Acceleration sensor calibration errors. (EC-1.80)
- Added support for the K0 stepping CPU.
- Improved: System hang with no display occurs when target system BIOS Setup is started using Hitachi JP1 AMT management software.
- Optimized docking control on Windows XP - An error message may be displayed if the following actions are performed - PC is placed in S4 (Hibernation), PC is docked, PC is powered on by pressing the power button or Hot-docked, Eject & Sleep is selected from the Start Menu, PC is undocked during S4, and the PC is powered on by pressing the Power Button.
- The thermal parameters were changed for the Tecra M11 3G model.
- Optimized USB Legacy control - If an external USB HDD is connected to the left-side USB port, the system may continually reboot.
- EC 1.70: Optimized USB wake-up control - If the system is put in an S3 state (Standby) and the mouse button is clicked continuously, the system may automatically reboot.
- Optimized the HDD password control for Compatibility Mode.
- Optimized the docking control for Windows 7.
- Improved the battery charge function while the battery has a very small amount of remaining capacity.
- Optimized the display control on Intel Graphics controller models with Windows XP.
- Fixed: An Unexpected Pop-up of PC Health Monitor may occur.
- Fixed: Bootup speed is slower when a DVD is in the optical disk drive (ODD).
- Changed the boot function so that a user can not use F12 boot if a supervisor password is enabled.
- Fixed: An unexpected pop-up of PC Health Monitor may occur.
- Fixed: Bootup speed is slow when a DVD is in the ODD.
- Added support for Arrandale Reference Code 1.30.
- Added support for Ibek-Peak Sighting #3622166.
- Improved: May not boot from certain USB memory devices.
- Initial production BIOS for these models.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.