ACPI Flash BIOS version 2.70 for Satellite P205/X205
- File: sp205v270.exe
- Version: 2.70
- Posted Date: 2011-01-25
- Release Date: 2010-12-22
- Other Versions
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Release Notes
- After the update completes, the computer will automatically shut down or restart.
- Power on the computer if it is off.
- While the "Toshiba" LOGO is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Change History
- Version 2.70 - 2010-12-22
- Fixed: After updating to Windows 7, the internal LCD may display abnormal horizontal lines.
- The Computrace Option ROM was updated to fix an issue where the Video and Touchpad driver will intermittently disappear in Windows 7 when Computrace is enabled.
- Implemented a workaround for an Intel ICH8M SATA Init LPM issue.
- Corrected: Black or blue screen when resuming from S3 with an ICH8 B2 chip.
- Implemented a workaround for an Intel ICH8M SATA Init LPM issue.
- Corrected: Black or blue screen when resuming from S3 with an ICH8 B2 chip.
- Disabled the Atheros XB63 WLAN ASPM L0s function.
- Updated Penryn CPU micro code.
- Updated Merom CPU micro code.
- Disabled the Atheros XB63 WLAN ASPM L0s function.
- Updated Penryn CPU micro code.
- Updated Merom CPU micro code.
- Added a BIOS workaround for Santa Rosa Penryn false thermal shutdowns that may occur in the S4 (hibernate) state.
- Corrected: BIOS Password is set automatically after updating the BIOS in Windows Vista x64 using Winflash64.
- Updated Penryn CPU T8100/T8300/T9300/T9500 Micro code.
- Added a BIOS workaround for Santa Rosa Penryn false thermtrip issues that may occur in the S3 (suspend) state.
- Modified the thermal function and added a fan table for Penryn CPUs.
- Corrected: The Express Card is not detected after a reboot on SLi models with 4GB of System Memory.
- Corrected: The Phoenix BIOS code was updated due to a USB flash boot issue with Robson.
- Corrected: An HDD password is requested after finger print log on.
- Corrected: Can not boot and enter the Operating System after connecting the TOSHIBA Dynadock via USB cable.
- Corrected: 3Com and emboot PXE boot failure on SLi models.
- Corrected: Can not boot from USB flash memory.
- Added: Penryn ES2 CPU micro code.
- Corrected: Garbage on the display when LCD CRT mode is selected and the CRT resolution is 1440x900 or higher. (ATI M72 VBIOS)
- Updated the ATI M72/M76 VBIOS to fine tune Hynix 512MB memory timing.
- Modified the Toshiba and Intel OSB logos.
- Disabled the Atheros XB72 WLAN L0s function.
- Updated the ATI M72 VBIOS BR25937.
- Corrected: Fn F5 Hot key does not change to CRT/TV mode without Toshiba Value Added Package (TVAP).
- Corrected: Beeping sound and no display when 4GB memory is inserted on the SLi platform.
- Corrected: Fn F6 and F7 function test problems on the SLi platform.
- A workaround was implemented to prevent a password from automatically being set by the computer.
- Added Computrace support for TAIS SKUs.
- Corrected: A password may be set during the DOS BIOS flash process.
- Added a workaround in to FLASH BIN to prevent an automatic (spontaneous) password set problem that occurs when EEPROM access fails using BIOS V1.50.
- Updated ATI M76 VBIOS to correct a Toshiba HD-DVD problem.
- Changed the initial fan voltage to 3V.
- Corrected Fn_Ctrl and Fn_Enter hotkey functions.
- Added a thermal table for SLi models.
- Added support for a thermal tool to show two VGA temperatures on SLI models.
- Updated the BIOS code to show the total memory capacity in the BIOS setup menu.
- Corrected: When "Power on Display" is set to "Auto-Selected" in the Setup Menu, nothing will be displayed on the external monitor.
- Added: HDMI function in the Toshiba Value Added Package (TVAP).
- Added: Winflash64 support.
- Updated: ATI M72M DDR2 VBIOS.
- Updated: Micro code for Celeron M540 CPU <10661h>.
- Corrected: Set the numeric keypad keys to be accepted in BIOS passwords.
- Corrected: Black screen after waking from Standby mode on certain models.
- Modified: The "Power on Display" item will be hidden from the Setup Menu on certain models.
- Corrected: The Fn+F5 display switch function doesn't work on certain models without TVAP.
- Modified: HDD password string "User Only" and "User+Master" on the Japanese language setup menu.
- Modified: Codec SSID for Dolby Home Theater on some models.
- Added: Nvidia NVIF TV mode support function due to a new driver requirement.
- Updated: NV 8ESE VBIOS.
- Modified: Verb table for changing EAPD behavior.
- Added: Intel Penryn CPU support.
- Added: NV-SLI VGA chipset support.
- Updated: Micro code for Penryn CPU <10671h>.
- Updated: Micro code for Merom CPU <6FBh>.
- Updated: ATI M72M DDR2 VBIOS version 25625 to fine tune the VRAM setting.
- Changed: Fn+F1 function scancode to press send makecode and release send break code when no TVAP is not installed.
- Corrected: Silent Mode can not be triggered after waking from Standby mode.
- Modified: The CoolingMethod status is stored when CoolingMethod is changed, and is restored after the Embedded Controller (EC) is initialized.
- "StickyKey "behavior was modified to avoid issues when switching between temporary mode and twice-lock mode.
- Modified: The Caps/Num lock LEDs will turned off when a KB reset command is received.
- Corrected: When the BIOS Setup Dynamic CPU frequency mode is set to "always Low", the CPU can not step down to 800Mhz.
- Updated: nVidia VBIOS can not turn on LG 17.1 WXGA+ (LP171WP4-TLB4) panels.
- Changed: Tj85 CPU thermal table.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.