Intel Display Driver
- File: os2011143a_inte...
- Version: 8.14.10.2330
- Posted Date: 2011-05-31
- Release Date: 2011-05-31
- Other Versions
-
Release Date: Version: 2010-11-18 8.14.10.2117
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
- This driver enhances the functionality of your display device and allows you to perform different settings, such as Color Management, Monitor Properties, or Overlay Control.
Change Points
- Fixed: When connected to a wide screen monitor (16:9) and set to display from the external monitor only, the display rolls from left to right.
Install Instructions
- Save the file to the Windows Desktop.
- Save all work in progress and close open applications.
- On the Windows Desktop, double-click the downloaded file to start the installation.
- Click OK, Unzip, then OK again.
- Click Yes if a User Account Control Window is displayed.
- Click Next at the Welcome screen.
- Click Yes at the License Agreement screen.
- Click Next at the Readme File Information screen.
- Click Next after installation completes.
- Select Yes, I want to restart this computer now then click Finish.
Version Verification
- Right-click on the Windows desktop and click Graphics Properties.
- Click the "i" icon at the top right corner of the window.
- Verify that the Driver Version is 8.14.10.2330.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.