ACPI Flash BIOS version 2.20 for mini notebook NB200/NB205 (PLL20U/23U/25U/28U)
- File: ll20v220.exe
- Version: 2.20
- Posted Date: 2012-02-03
- Release Date: 2011-03-30
- Other Versions
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Release Notes
- After the update completes, the computer will automatically shut down or restart.
- Power on the computer if it is off.
- While the "Toshiba" LOGO is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Change History
- Version 2.20 - 2011-03-30
- Disabled WLAN L0s by vendor request.
- Fixed: Screen scrolls when the computer is idle.
- Improved the BIOS flash algorithm to prevent EEPROM data corruption. (EC-2.00)
- Modified a PN number for a Japanese SKU default language setting.
- Fixed: Will check that AC & Battery exists when flashing the BIOS.
- Added a new 3G logo for Chinese models.
- Fixed: Video and Touchpad drivers intermittently get banged out in Windows 7 when Computrace is enabled.
- Modified the F5 hotkey function for WIN7 the WINP function.
- Modified: PHM Backlight ON/Off NO event.
- Updated the Kill-Switch function per the ACPI BIOS spec.
- Fixed: When the Sleep&Charge mode is changed from mode 4 to disable, the Sleep&Charge Utility will show Enabled and Mode1.
- Modified: Force the Bluetooth (BT) power on when running Linux.
- Disabled the unused slots clock to save battery power.
- Modified: BIOS Setup string.
- Added new WLAN support.
- Added the computrace function to support a European SKU.
- Fixed: The user password can not be changed when the Supervisor password is used to enter setup.
- A change was made to meet the setup menu specification for the kill switch function.
- Updated: BIOS Setup menu string.
- Modified: Default Language for a Japanese SKU.
- Added: NON_OS function support.
- Fixed: System cannot wake on LAN continuously after waking from S3 in Windows Vista.
- Fixed: Fn+1 and Fn+2 functions are reversed in Windows Vista.
- Modified: Touch Pad on/off method for hotkeys to prevent a conflict with the ALPS touchpad (TP) driver – when a USB mouse is plugged in/out, the TP function is disabled/enabled.
- Modified: T-diode calibration algorithm in Windows Vista.
- Modified: WOL is always enabled in S3 and S4 modes in Linux.
- Modified: Brightness table.
- Modified: Fan control setting.
- Modified: ACOP function.
- Added a WinBound thermal sensor function.
- Disabled: LAN power on in DC mode for Linux.
- Modified: When System shuts down the 3G device Status is stored in EEPROM.
- Modified: HDP function (resume from S3).
- Added: Win+P key for Windows 7.
- Initial production BIOS for these models.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.