nVidia Display Driver
- File: os2012129a_tc90...
- Version: 296.31
- Posted Date: 2012-05-10
- Release Date: 2012-05-10
- Other Versions
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
- This driver enhances the functionality of your display device and allows you to perform different settings, such as Color Management, Monitor Properties or Overlay Control.
Notes
- This Driver is for NON-3D Windows 7 64-bit models only.
Change Point
- Adds support for some new games.
Driver Install Instructions
- Save the file to the Windows Desktop:
- Save all work in progress and close open applications.
- On the Windows Desktop, double-click the downloaded file to start the installation.
- Click Start at the TOSHIBA Archive Extractor window.
- Click Yes if a User Account Control window is displayed.
- Click Agree and Continue to accept the software license agreement.
- Select Express and click Next. The installation will begin.
- Click Close to complete the update.
- Please restart Windows manually to apply the driver change.
Driver Version Verification
- From the Start menu type PC Diagnostic Tool and press Enter. (All Programs -> Toshiba -> Utilities)
- Verify that the Video version is 8.17.12.9631.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.