Toshiba ConfigFree Utility
- File: tc00163701h.exe
- Version: 8.0.43n
- Posted Date: 2012-05-17
- Release Date: 2011-10-24
- Other Versions
-
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
-
ConfigFree® is a set of utilities that makes it easy to control communication devices and network connections. ConfigFree also lets you identify communication problems and create profiles for easy switching between locations and communication networks.
To access ConfigFree go to START > ALL PROGRAMS > TOSHIBA > NETWORK & CONNECTIVITY > CONFIG FREE.
ConfigFree allows you to perform the following:
- Use Connectivity Doctor to quickly fix any network connection problems.
- Create ConfigFree profiles for automatic switching between preset network settings and devices, even if there is a change in the network environment.
- Automatic switching between several wireless LAN environments.
- Automatic switching to a wireless LAN if the cable is disconnected when using both a wired and wireless LAN.
- You can also easily switch LAN environments manually.
You may have to add the ConfigFree gadget to your computer to allow you to use ConfigFree features.
To add the ConfigFree gadget:
- Click the Start menu.
- Enter "Configfree" into the search field.
- Click "Add ConfigFree Gadgets" in the search results.
-
The Add ConfigFree Gadgets window will open.
- Add the desired gadget and click "Add".
-
If Add Windows Sidebar Gadget is selected, the gadget will display on your desktop.
- The dots on the gadget are available connection points. If you are connected to one, a line will conne
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.