Download Toshiba Drivers and Utilities for Windows 8
- Document ID: 98083956
- Posted Date: 2012-08-31
- Last Updated: 2012-08-31
- Distribution: View Public Website
- Information
Toshiba recommends using the Toshiba Upgrade Assistant when upgrading to Windows 8 to support ongoing use of Toshiba provided features and functionality.
If you prefer to manually upgrade to Windows 8, Toshiba provides instructions to assist you. These instructions help you prepare for the upgrade process, including removal of Toshiba-supplied software that should be uninstalled prior to starting the upgrade. The instructions also include information about installation of Toshiba-supplied software after the Windows 8 upgrade is complete, including a list of each software components to be downloaded and installed. There are typically many components that have to be manually and individually downloaded using this process, so Toshiba strongly recommends using the upgrade assistant to ease this process.
The individual software components for Windows 8 and the manual upgrade instructions are available first by verifying that your laptop model is supported by Toshiba for upgrade to Windows 8. Return to the Toshiba Windows 8 Upgrade Information Web site and follow the instructions under the heading "How to upgrade to Windows 8".
Click here for general instructions on navigating the Toshiba Support website for Downloads and other support content.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.