ACPI Flash BIOS version 1.10 for Satellite C845D/L845D (PSC9A*/PSKEG*)
- File: sc9av110.exe
- Version: 1.10
- Posted Date: 2012-06-29
- Release Date: 2012-05-17
- Other Versions
-
Release Date: Version: 2012-06-11 1.00
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Release Notes
- The BIOS update will force the computer to shut down or restart. Please make sure to save all work in progress before starting BIOS updates.
- Power on the computer if it is off.
- While the "Toshiba" LOGO is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Change History
- Version 1.10 - 2012-05-17
- Added: GPIO50 definition for HDMI detection of UMA SKUs.
- Disabled ALPM.
- Initial production BIOS release for these models.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.