ACPI Flash BIOS version 2.70 for Satellite/Sat Pro L640/L645/L745 (PSK0G*/H*/L* PSK6V*)



File: sk0gv270.exe




Version: 2.70
 
Posted Date: 2012-08-15

 

Release Date: 2012-07-03

 

Other Versions

 

Package
WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
Description

Release Notes

  • After the update completes, the computer will automatically shut down or restart.
  • Power on the computer if it is off.
  • While the "Toshiba" LOGO is displayed, press the F2 function key to start BIOS Setup.
  • Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
  • Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.

Change History

    Version 2.70 - 2012-07-03
    • Implemented changes for the Windows 8 upgrade.
    • Updated: New Keyboard ID for Windows 8.
    Version 2.60 - 2012-05-21
    • Updated the EC.
    Version 2.50 - 2012-04-12
    • Updated the EC to implement battery charge improvements.
    Version 2.30 - 2011-03-23
    • Updated: Video BIOS for Satellite L740 models sold outside of the U.S. and Latin America.
    • Fixed: ESATA device is disabled by default on Satellite L640 models.
    Version 2.20 - 2011-03-07
    • Added: CPU throttling function for a diagnostic test.
    • Fixed: USB device can not be recognized.
    • Updated: Video BIOS (VBIOS) for Satellite L640/L645 - ATI HD 5430 from BR37218.001 to BR39975.001, ATI HD 5730 from BR37226.001 to BR39976.001.
    • Combined Satellite L640/L645 & Satellite L740/L745 BIOSs starting with this version. Note: Satellite L750/L750 models are not sold in the U.S. or Latin America at this time.
    Version 2.00 - 2011-03-08
    • Updated ATI Mobility Radeon (M92, Madison, and Park) Video BIOSs to support new Hynix and Samsung Video RAM dies.
    Version 1.90 - 2010-12-31
    • Updated the PXE ROM from v2.0.1.9 to v2.0.2.7.
    Version 1.70 - 2010-09-15
    • When is Fastboot enabled with no HDD connected, "No boot device" is displayed.
    • Fixed: User password shows "password fail" if HWsetup sets the keypad "/" key as part of the password.
    Version 1.60 - 2010-08-09
    • Changed the M92 VBIOS from BR37094.004 to BR37094.003.
    • Fixed: SmartDE shows an error message when booting from the ODD.
    • Disabled the Power Button while flashing the BIOS.
    • Fixed: MIC device doesn't work in the operating system when fastboot is enabled.
    • Updated the MRC code.
    Version 1.40 - 2010-06-03
    • Fixed: An abnormal login screen appears after rotating the display 90 or 180 degrees, then waking from Sleep (S3 mode) using a USB mouse or keyboard.
    • Fixed: The system will show an error message if the power button is pressed to force a shutdown on P6000 CPU models.
    Version 1.30 - 2010-05-06
    • Added support for the D2D function in Fast Boot Mode.
    • Added support for Arrandale K0 stepping CPU and EMRR function.
    • Removed ALPS TouchPad support.
    • Fixed: The Owner String in HWSetup can not be seen when Fast Boot is enabled..
    • Fixed: An incorrect battery serial number is reported to the OS.
    • Fixed: The computer hangs in Windows XP when Toshiba Power Saver is installed.
    • Updated the M96 VBIOS from BR036040.001 to BR36040.002.
    • Fixed: Updated the AHCI ROM to prevent system hangs while using the SmartDE HDD encryption tool.
    • Updated the Madison (ATI) VBIOS to BR37218_001.
    • Fixed: Windows Mobility Center disappear when the battery is removed.
    • Fixed: Can not boot to DOS on a USB device when Fast Boot is enabled.
    • Fixed: The BIOS may incorrectly report the presence of an HDMI port in Windows XP.
    • Fixed: The Toshiba CCD utility does not turn on automatically after resuming from Hibernation (S4) in Windows XP.
    • Updated the M92 VBIOS from BR37094.001 to BR37094.004.
    • Updated the Park (ATI) VBIOS to BR37226.00.
    • Added support for the P6000 CPU.
    • Updated: DMI Type1 0x19 string.
    Version 1.10 - 2010-03-26
    • Initial production release.
Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.