ACPI Flash BIOS version 2.00 for mini notebook NB505 (PLL50U)
- File: ll50v200.exe
- Version: 2.00
- Posted Date: 2012-08-16
- Release Date: 2012-07-31
- Other Versions
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Release Notes
- After the update completes, the computer will automatically shut down or restart.
- Power on the computer if it is off.
- While the "Toshiba" LOGO is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Change History
- Version 2.00 - 2012-07-31
- Fixed: PXE hang on localboot in Linux.
- Fixed: Optical Disk Drive is not detected during POST.
- Added support for the Samsung LTN101NT07-T01 LCD panel.
- EC: Added LTN101NT07-T01 Panel Settings.
- 1. Disabled ASPM L0s on Intel and other WLAN devices.
- Addressed a 3G card (F5521) POST time delay. Note: 3G models were not sold in the United States or Latin America.
- 1. Fixed: System hangs when using the Intel Wireless LAN card to connect to the internet. Note: This update is not recommended for PLL50U-xxxxxx owners at this time because Intel Wireless LAN cards have not been used in NB500/NB505 models sold in the United States and Latin America.
- Fixed: HB116 WLAN card hang.
- Added support for the Askey WB195 combo card - WLL6220B-D4.
- EC-1.40: Modified the USB over current protection when the EC is in the deep sleep mode.
- EC-1.40: Removed the low battery beep alarm.
- EC-1.40: Modified Fn+F9 behavior.
- Modified the battery gas gauge.
- EC-1.30: Added AC adapter capacity information.
- Initial production BIOS.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.