Toshiba Value Added Package (64bit)



File: TC30485400D.exe




Version: 1.6.0130.640204
 
Posted Date: 2012-09-12

 

Release Date: 2012-09-12

 

Other Versions
Release Date:Version:
2011-11-281.6.9.64
2011-10-041.6.9.64
2011-12-191.6.9
2011-11-041.6.9
2011-08-161.6.3.64WW2
2011-08-221.6.3.64K
2011-10-041.6.3.64
2011-08-161.6.3.64
2011-10-041.6.3
2011-10-041.6.3
2012-05-111.6.19.64
2012-01-091.6.16.64
2011-12-151.6.16.64
2011-12-151.6.16
2011-09-061.6.1.64G
2011-08-021.6.1.64
2011-10-041.6.1
2011-10-041.6.1
2012-08-161.6.0130.640202
2012-09-121.6.0130.320204
2012-08-161.6.0130.320202
2012-05-301.6.0128.640201
2012-05-301.6.0128.320201
2012-06-011.6.0028.640202
2012-04-271.6.0027.640202
2012-05-181.6.0027.320202
2012-05-091.6.0026.640202
2012-05-101.6.0026.320202
2012-05-301.6.0025.640205
2012-04-091.6.0025.640205
2012-04-191.6.0023.640204
2012-06-181.6.0023.320204
2012-05-311.6.0022.640207
2012-04-181.6.0022.640207
2012-02-291.6.0021.640203
2012-02-271.6.0021.640203
2012-04-241.6.0021.320203
2011-04-271.5.4_64WW
2011-09-281.5.4.64
2011-04-041.5.4.64
2011-09-281.5.4
2011-09-271.5.3_64
2011-03-071.5.3_64
2011-03-071.5.3
2011-04-041.5.1_64
2011-08-031.5.14.64
2011-05-251.5.12.64
2011-05-251.5.11.64
2011-04-271.5.10.64
2011-05-311.5.10
2011-09-271.4.4_64
2011-01-251.4.1_64G
2011-01-111.4.1_64
2010-06-211.3.6_64
2010-06-211.3.4_64
2010-06-211.3.3_64
2010-11-111.3.3
2010-06-211.3.2_64
2010-12-271.3.23_64
2011-09-271.3.22_64
2010-12-271.3.22_64
2011-09-281.3.22
2011-09-291.3.20
2010-10-181.3.19_64
2011-10-041.3.19
2010-11-221.3.14_64K3
2010-09-011.3.14_64K2
2010-08-101.3.14_64
2010-06-231.3.13_64
2010-07-131.3.11_64
2009-07-271.2.8_Update4
2009-06-291.2.8_64
2009-06-031.2.8_64
2010-09-011.2.40_64
2010-06-211.2.39_64
2009-11-121.2.34_64
2009-12-161.2.33_64
2009-12-161.2.33
2010-01-151.2.32_64
2010-01-251.2.32
2009-10-201.2.28
2009-10-201.2.27_64
2009-09-031.2.27_64
2009-09-031.2.27
2009-10-071.2.26_64
2009-10-081.2.26
2009-07-011.2.14_64T
2009-07-011.2.14.T
2009-07-171.2.10
2008-01-031.1.7
2007-06-201.0.21

 

Package
WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
Description

TOSHIBA VALUE ADDED PACKAGE

The Toshiba Value Added Package (TVAP) provides an essential link to system resources required by several TOSHIBA original program components for access to BIOS functions etc, such as:

  • TOSHIBA eco Utility provides extended power control options to our customers over devices in Toshiba notebooks. Reduction in power consumption by switching to optimum power settings based on plugged-in or on battery power machine status, or remaining battery power percentage.
  • TOSHIBA HWSetup lets you customize your hardware settings according to the way that you work with your computer and the peripherals you use.
  • TOSHIBA Password Utility lets you set and maintain password security that restricts access to the computer.
  • TOSHIBA Flash Cards provides additional Hotkey (Function Fn keys) functionality to Toshiba notebooks and includes an intelligent user interface (UI) in the form of a graphical drop-down invoked by hotkey operation. This improves the user experience by allowing them to visually identify current status and available options at time of selection, saving them time spent blindly moving between the hot-key options to find the one they need.
  • TOSHIBA PC Diagnostic Tool can display the basic information of a computer and diagnose simple issues using Windows built-in toolset.

TVAP should be installed before other Toshiba Utility files to ensure their proper functioning.

If TVAP is not installed on your computer, you can verify if it is available for your specific model under "Downloads" on the TOSHIBA support web site (support.toshiba.com).

Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.