Toshiba Media Controller Plug-in

WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
This is a TOSHIBA Media Controller Plug-in update.

Change Points

  1. Eliminates the following error after updating the Adobe Flash Player to version "The Adobe Flash Player installed on your PC is not supported by TOSHIBA Media Controller Plug-in. TOSHIBA Media Controller Plug-in failed to start.
    This error occurs when attempting to forward movie play back to an external display.

Install Instructions

  1. Save the downloaded file to the Windows Desktop.
  2. Save all work in progress and close open applications.
  3. On the Windows Desktop, double-click the downloaded file to start the installation.
  4. Click Start when the TOSHIBA Archive Extractor window is displayed.
  5. Click Yes to continue if a User Account Control window is displayed.
  6. Click Next at the TOSHIBA Media Controller Plug-in InstallShield Wizard.
  7. Click Install to start the installation.
  8. Click Finish to complete the installation.

Version Verification

  1. Click Start, type Add or Remove Programs, then press Enter.
  2. Verify that the TOSHIBA Media Controller Plug-in application is version

Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Toshiba end-user license agreement both of which you can view before downloading any such software.