ACPI Flash BIOS version 2.80 for Satellite P750/P755 (PSAY1x/PSAY3x)
- File: say1v280.exe
- Version: 2.80
- Posted Date: 2012-11-29
- Release Date: 2012-11-23
- Other Versions
-
Release Date: Version: 2012-07-10 2.60 2012-02-07 2.40 2011-09-01 2.10 2011-09-01 2.00 2011-05-26 1.90 2011-05-17 1.80
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Release Notes
- For CD-ROM BIOS updates: Type BIOS then press enter at the C:\ prompt.
- For all updates: After the update completes, the computer will automatically shut down or restart.
- Power on the computer if it is off.
- While the "TOSHIBA" logo is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Change History
- Version 2.80 - 2012-11-23
- Fixed: The computer will hang at the Windows logo when "Fast Boot" is enabled.
- Fixed: after checking "Enable Sleep and Charge" in the TOSHIBA Sleep Utility, the computer will not restart by pressing F10 in BIOS Setup - Windows 8 computers only.
- Updated: ME Firmware to V7.1.52.1176.
- Updated: NVIDIA N12P-GS VBIOS to V70.08.4A.00.22.
- Adjusted the TV-tuner step-two low limit value to match the fan table setting.
- Made a change to return correct HCI function data when RTC wake is disabled.
- Set the default boot speed to "Fast" and enabled the Legacy USB function for Toshiba America Best Buy SKUs.
- Modified the Hi-Speed Start function to notify Toshiba Value Added package (TVAP) when the power button is pressed or the lid is closed.
- Added an Intel update solution for the "PCIe Presence Detect State May Not Be Accurate after a Warm Reset" issue.
- Updated: CPU Microcode to Rev 0x1A.
- Fixed: Noise when the eco or illumination on/off buttons are pressed.
- Added: Hybrid Boot feature.
- Added: Peak Shift feature.
- Fixed: User/Supervisor Password entry box is positioned behind the owner string window.
- Fixed: The Language setting in the BIOS Setup Utility is saved even though "Exit Discarding Changes" was selected.
- Initial production BIOS for this model.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.