ACPI Flash BIOS version 2.20 for Satellite P740/P745 (PSMQ1U/PSMQ3U)
- File: smq1v220.exe
- Version: 2.20
- Posted Date: 2012-11-30
- Release Date: 2012-11-23
- Other Versions
-
Release Date: Version: 2012-02-14 1.90 2011-08-25 1.70 2011-08-25 1.60 2011-08-25 1.40 2011-08-25 1.30
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
Release Notes
- For CD-ROM BIOS updates: Type BIOS then press enter at the C:\ prompt.
- For all updates: After the update completes, the computer will automatically shut down or restart.
- Power on the computer if it is off.
- While the "TOSHIBA" logo is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Change History
- Version 2.20 - 2012-11-23
- The computer will hang at the Windows logo when "Fast Boot" is enabled.
- Fixed: after checking "Enable Sleep and Charge" in the TOSHIBA Sleep Utility, the computer will not restart by pressing F10 in BIOS Setup - Windows 8 computers only.
- Updated: ME Firmware to 7.1.52.1176.
- Set the default boot speed to "Fast" and enabled the Legacy USB function for Toshiba America Best Buy SKUs.
- Added an Intel update solution for a "PCIe Presence Detect State May Not Be Accurate after a Warm Reset" issue.
- Updated: CPU Microcode to Rev 0x1A.
- Updated: LAN PXE ROM.
- Fixed: Noise when the eco or illumination on/off buttons are pressed.
- Fixed: When Optimus is enabled the fan will intermittently turn on even when the CPU temperature is low.
- Modified the F1 Help string from "-><-" to "<-->".
- Modified: Boot menu is grayed out when a user password is used in the Setup Menu.
- Updated: ME Firmware for the IPT function.
- Initial production BIOS for these models.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.