nVidia Display Driver (64bit)
- File: os2012401a_tc50...
- Version: 306.46
- Posted Date: 2013-01-09
- Release Date: 2013-01-09
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
- This driver enhances the functionality of your display device and allows you to perform different settings, such as Color Management, Monitor Properties or Overlay Control.
Notes
- Version 9.18.13.646 for Windows 8 3D platforms only.
Change Point
- Fixed: Warning message while playing 3D BD or DVD discs, and changing between 2D and 3D modes in TOSHIBA Blu-ray Disc Player in Windows 8: "Warning: Attempt to run stereoscopic 3D in a nonstereo display mode. Please change to an acceptable mode."
Driver Install Instructions
- Save the file to the Windows Desktop:
- Save all work in progress and close open applications.
- On the Windows Desktop, double-click the downloaded file to start the installation.
- Click Start at the TOSHIBA Archive Extractor window.
- Click Yes if a User Account Control window is displayed.
- Click Agree and Continue to accept the software license agreement.
- Select Express and click Next. The installation will begin.
- Click Close to complete the update.
- Please restart Windows manually to apply the driver change.
Driver Version Verification
- From the Start menu type PC Diagnostic Tool and press Enter. (All Programs -> Toshiba -> Utilities)
- Verify that the Video version is 9.18.13.646.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.