ACPI Flash BIOS version 6.30 for Satellite/Qosmio P870/P875/X870/X875



File: splav630.exe




Version: 6.30
 
Posted Date: 2013-02-21

 

Release Date: 2013-01-31

 

Other Versions

 

Package
WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
Description

Release Notes

  • For CD-ROM BIOS updates in Windows 8 models: (1) Shut down the system while pressing the SHIFT key to completely power off. (2) Power on while pressing F2 to enter the BIOS Setup Menu. (3) Go to the Security tab and set the "Secure Boot" setting to "Disabled". (4) Go to the Advanced tab, enter "System Configuration" and set the Boot Mode to "CSM Boot." (5) Press F10 to save and exit. (6) Boot from the BIOS CD-ROM and type FLASH at the C:\ prompt. (7) After the BIOS update has completed, restore the Boot Mode setting to "UEFI Boot" and the Secure Boot setting to Enabled.
  • For CD-ROM BIOS updates in Windows 7 models: Type FLASH then press enter at the C:\ prompt.
  • For all updates: The BIOS update will force the computer to shut down or restart. Please make sure to save all work in progress before starting BIOS updates.
  • Power on the computer if it is off.
  • While the "TOSHIBA" logo is displayed, press the F2 function key to start BIOS Setup.
  • Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
  • Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.

Change History

    Version 6.30 - 2013-01-31
    • Fixed: System hangs after settings are changed by TSS.
    • Added: CER key for a Smart DE issue.
    Version 6.20 - 2012-12-26
    • Changed: Lid wake up capability.
    • Added: Support for the AUO B173HW02 V0 FHD LCD panel.
    Version 6.10 - 2012-09-26
    • Updated: IVB 306A9 Microcode from M12306A9_00000013 to M12306A9_00000015.
    Version 6.00 - 2012-09-05
    • First release for Windows 8.
    Version 1.50 - 2012-07-04
    • Updated: ME firmware.
    Version 1.30 - 2012-05-10
    • Added: NVIDIA N13P_GS VBIOS.
    • Updated: "Boot Speed" default set to "Fast" on Best Buy models when the DMI 6th & 30th characters are "U"&"P".
    Version 1.20 - 2012-04-27
    • Updated: Chief River, Maho Bay, Dashboard final, SA1.5.
    • Updated: Ivy Bridge Screen Flicker Sighting Alert Rev1_0, SA 1.5.
    • Updated: Ivy Bridge Graphics Cache Config Sighting Alert Rev 1_0
    • Modified: Discrete VGA SKU DC max power from 55W to 73W.
    • Updated: Sandy Bridge (SNB) Microcode to M12206A7_00000026.
    • Fixed: ODD disappears after setting the SATA Interface to "Battery life" and resuming from Sleep (S3).
    Version 1.10 - 2012-04-02
    • Initial production BIOS for these models.
Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.