Intel Wireless Display
- File: os2013064a_tc00...
- Version: 3.5.41.0
- Posted Date: 2013-04-05
- Release Date: 2013-04-05
- Other Versions
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
- This is the Intel Wireless Display Driver.
Note: Intel PROSet and Wireless LAN Driver versions 15.5.7/15.5.7.52 should be installed with this update.
Intel Proset and Wireless LAN Driver versions 15.5.7/15.5.7.52 (64-bit). Intel Proset and Wireless LAN Driver versions 15.5.7/15.5.7.52 (32-bit).
Change Points
- Fixed: Localization issues on non-English operating systems.
- Improved: Intermittently displays "not responding".
- Improved: AV quality.
- Improved: Connection reliability.
- Fixed: Yellow bang in Device Manager when the calendar date is later than Jan 1st 2013.
Install Instructions
- Save the file to the Windows Desktop.
- Save all work in progress and close open applications.
- On the Windows Desktop, double-click the downloaded file to start the installation.
- Click the Start button when the Toshiba Archive Extractor window is displayed.
- Click Start at the TOSHIBA Archive Extractor window.
- Click Yes if a User Account Control window is displayed.
- Click Upgrade at the Intel(R) WiDi window.
- Click "I accept the terms in the license agreement" then click Next.
- Click Finish.
- Click Yes to restart the computer.
Version Verification
- In Control Panel, Programs and Features:
- Verify that the Intel (R) WiDi version is 3.5.41.0.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.