Toshiba eco Utility
- File: tc30552400f.exe
- Version: 2.0.4.6405
- Posted Date: 2013-04-26
- Other Versions
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
-
Some laptops are equipped with "eco mode". This mode slightly lowers performance of some devices to reduce electric power consumption. You can realize measurable power savings by using it continuously. TOSHIBA eco Utility helps you monitor your power savings by showing approximate real time power consumption. Furthermore, it shows approximate accumulated power consumption and approximate accumulated power savings when using eco mode daily, weekly, and monthly. The utility also shows the approximate accumulated CO2 emission and savings while using eco mode. You can track power savings by using eco mode continuously.
eco Mode sets the conditions described below. If you deviate from these settings, e.g., if you turn up the monitor brightness or turn on the LED illumination (*1), it will no longer be eco mode.
eco power plan is used for eco Mode. It has the following settings by default. These settings are in addition to the standard Power saver plan settings of Windows.
On AC adaptor plugged in:
It changes the display brightness to Level-4, changes the dimmed display brightness to Level-1 (*4), turns off the LED illumination (*1) and the keyboard backlight (*2), changes the time before dim the monitor to 2 minute (*4), changes the time before the monitor turns off to 5 minutes, changes the time before the hard disk turns off to 5 minutes, and changes the time before the system enters sleep to 10 minutes.
On Battery:
It changes the display brightness to Level-3, changes the dimmed display brightness to Level-1 (*4), turns off the LED illumination (*1) and the keyboard backlight (*2), changes the time before dim the monitor to 1 minute (*4), changes the time before the monitor turns off to 3 minutes (2 minutes, if models with Windows 7 installed), changes the time before the hard disk drive turns off to 3 minutes, and changes the time before the system enters into sleep mode to 5 minutes."
If you change the power plan to "eco", your PC is on eco mode.*1: Only on models that support LED illumination
*2: Only on models that support Keyboard backlight
*3: Only on models that include the eco Button
*4: Only on models with Windows7 installedTo open the TOSHIBA eco utility:
- Click the Start menu.
- Enter "eco" into the search field.
- Click "eco Utility" in the search results.
-
Please read the information in the first box, select "Agee" and click "OK".
-
The TOSHIBA eco Utility will open allowing you monitor power consumption and set preferences.
- To learn more about the TOSHIBA eco Utility, click "Help" at the bottom of the screen
CLICK HERE and Refer to your Owner's Manual for additional information on the TOSHIBA eco Utility.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.