Android WinUsb Driver
- Package
- PKZip file can be extracted with WinZip, PKZip, or equivalent UnZip utility. Save file to a directory on your HDD and UnZip.
- Description
- - Operating environment
·Windows(R) XP SP3 or later (32bit Version)
·Windows(R) 7 SP1 or later (32 bit/64 bit Version)
* Computer is needed to have USB comformed USB1.1 or later.
- How to install Android WinUsb Driver
1) Unzip usb_driver.zip at computer to be installed driver.
2) Tap [Build number] 7 times at [Settings]-[About tablet] screen at tablet,then [{} Developer options] menu is displayed.
3) Check [USB debugging] checkbox at [{} Developer options] screen.
4) Connect your tablet to your computer's USB port.
5) Install Android WinUsb Driver driver from hardware update wizard.
[Windows XP]
1) Connect your tablet to your computer's USB port.
Windows will detect the tablet and launch the Hardware Update Wizard.
2) Select [No, not this time] and click [Next].
3) Select [Install from a list or specific location (Advanced)] and click [Next].
4) Select [Don't search. I will choose the driver to install] and click [Next].
5) If you are prompted to Select a hardware type,keep the default selection [Show All Devices], and click [Next].
6) Click [Have Disk], click [Browse] and specify the folder of unzipped usb_driver.zip.
7) Click [Next] in the wizard.
8) Click [Finish].
[Windows 7]
1) Connect your tablet to your computer's USB port.
2) Open device manager at your computer.
3) Right-click the device name and Select [Update Driver Software..].
This will launch the Hardware Update Wizard.
4) Select [Browse my computer for driver software].
5) Select [Let me pick from a list of device drivers on my computer]
6) Click [Have Disk], click [Browse] and specify the folder of unzipped usb_driver.zip
7) Click [Next] in the wizard.
8) Click [Install this driver software anyway]
9) Click [Close]
- ADB connection of your computer and tablet
* Download latest Android SDK from following.
http://developer.android.com/sdk/index.html
1) Install Android WinUsb Driver by "How to install Android WinUsb Driver".
2) Confirm ADB connection of your computer and tablet.
[ADB connection confirmation]
1) Run command prompt at your computer.
2) Move to platform-tools folder under Android SDK folder.
3) ADB connection is established, if HEX string is displayed under [List of devices attached], when [adb devices] command is executed.
- Note
- This driver doesn't warranted for all computer,
if the computer is adopted to target computer and OS.
- FAQ
Q. USB Composite Device is recognized as MTP when you connect your tablet to your computer's USB port.
A1. Confirm that [USB debugging] checkbox is checked at tablet.
For details, see the steps 1) - 3) in "How to install Android WinUsb Driver".
A2. Update driver from MTP to USB composite device at device manager.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.