Android WinUsb Driver
- File: TC00543100B.zip
- Posted Date: 2014-02-14
- Release Date: 2014-02-14
Accessory Accessory |
- Android WinUsb Driver
Operating environment
Windows(R) XP SP3 or later (32bit Version)
Windows(R) 7 SP1 or later (32 bit/64 bit Version)
* Computer is needed to have USB comformed USB1.1 or later.How to install Android WinUsb Driver
1) Unzip usb_driver.zip at computer to be installed driver.
2) Tap [Build number] 7 times at [Settings]-[About tablet] screen at tablet,then [{} Developer options] menu is displayed.
3) Check [USB debugging] checkbox at [{} Developer options] screen.
4) Connect your tablet to your computer's USB port.
5) Install Android WinUsb Driver driver from hardware update wizard.[Windows XP]
1) Connect your tablet to your computer's USB port.
Windows will detect the tablet and launch the Hardware Update Wizard.
2) Select [No, not this time] and click [Next].
3) Select [Install from a list or specific location (Advanced)] and click [Next].
4) Select [Don't search. I will choose the driver to install] and click [Next].
5) If you are prompted to Select a hardware type,keep the default selection [Show All Devices], and click [Next].
6) Click [Have Disk], click [Browse] and specify the folder of unzipped usb_driver.zip.
7) Click [Next] in the wizard.
8) Click [Finish].[Windows 7]
1) Connect your tablet to your computer's USB port.
2) Open device manager at your computer.
3) Right-click the device name and Select [Update Driver Software..].
This will launch the Hardware Update Wizard.
4) Select [Browse my computer for driver software].
5) Select [Let me pick from a list of device drivers on my computer]
6) Click [Have Disk], click [Browse] and specify the folder of unzipped usb_driver.zip
7) Click [Next] in the wizard.
8) Click [Install this driver software anyway]
9) Click [Close]ADB connection of your computer and tablet
* Download latest Android SDK from http://developer.android.com/sdk/index.html
1) Install Android WinUsb Driver by "How to install Android WinUsb Driver".
2) Confirm ADB connection of your computer and tablet.
[ADB connection confirmation]
1) Run command prompt at your computer.
2) Move to platform-tools folder under Android SDK folder.
3) ADB connection is established, if HEX string is displayed under [List of devices attached], when [adb devices] command is executed.Note
- This driver doesn't warranted for all computer, if the computer is adopted to target computer and OS.FAQ
Q. USB Composite Device is recognized as MTP when you connect your tablet to your computer's USB port.
A1. Confirm that [USB debugging] checkbox is checked at tablet.
For details, see the steps 1 - 3 in "How to install Android WinUsb Driver".
A2. Update driver from MTP to USB composite device at device manager.- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.