nVidia Display Driver
- File: OS2013427C_TC50...
- Version: 9.18.13.2765
- Posted Date: 2014-03-03
- Release Date: 2014-03-03
- Other Versions
-
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
-
This driver enhances the functionality of your display device.
Change Point
- Fixed the concern of vulnerabilities for some of the NVIDIA Graphics Controllers.
- Please see "CVE-2013-5987" in below web site about detailed information.
- English site: http://www.nvidia.com/security
- Chinese site: http://www.nvidia.cn/object/product-security-cn.html
Driver Install Instructions
- Download and save the file to the Windows Desktop:
- Save all work in progress and close open applications.
- On the Windows Desktop, double-click the downloaded file to start the installation.
- Press Start at the TOSHIBA Archive Extractor window.
- Press Yes if a User Account Control window is displayed.
- Press Agree and Continue to accept the software license agreement.
- Select Express and press Next. The installation will begin.
- Press Close to complete the update.
- Please restart Windows manually to apply the driver change.
Driver Version Verification
- Open Control Panel.
- Select Programs then Uninstall a program.
- Find NVIDIA Driver.
- Verify that the Driver Version is 9.18.13.2765.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.