Toshiba Display Utility
- File: tc00583400e.exe
- Version: 1.1.16.0
- Posted Date: 2014-03-13
- Other Versions
-
Release Date: Version: 2015-03-09 v1.2.10.0 2015-07-29 2.0.1.0_B 2014-12-02 1.2.6.0 2014-04-17 1.1.17.0
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
- This is a TOSHIBA Display Utility version 1.1.16.0 package.
Change Points
- Fixed: When per-display DPI scaling is used, after changing to clone mode or secondary only mode, the fit button may not be displayed in the Explorer window.
Release Notes
- When you update to a new version, the previous version of Split Screen plugin is uninstalled.
- If you want to use the Split Screen function continuously,please install Split Screen plugin per instructions below:
- Launch TOSHIBA Display Utility.
- Press [Install Split Screen] at the [Split Screen] tab.
- When you update to a new version, Resolution+ Setting, Demo Mode, and the Application Settings of the current version will be reset.
- When several user accounts exist, Skype for Windows8.1 is not displayed in the Application Setting window until you use Windows Skype for Windows 8.1.
Installation Instructions
- Save this file to a convenient location such as the Windows Desktop
- Save all work in progress and close open applications.
- From the Windows Desktop, run the downloaded file to start the installation.
- If a User Account Control or Open File message is displayed, press Continue.
- Press the Start button at the Toshiba Archive Extractor window.
- Press the Next button at the InstallShield Wizard screen.
- Press the Finish button when the installation completes.
Driver Version Verification
- Open Control Panel.
- Select Programs - Uninstall a program.
- Find TOSHIBA Display Utility.
- Verify that the version is 1.1.16.0.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.