DisplayLink dynadock and USB Monitor driver V7.6 M0 for Windows 7, 8, and 8.1
- File: displaylink_NR-...
- Version: 7.6.55102.0
- Posted Date: 2014-04-28
- Release Date: 2014-04-28
- Other Versions
-
dynadock PA3541U-2PRP dynadock VGA |
dynadock PA3542U-2PRP dynadock DVI |
dynadock PA3575U-1PRP dynadock U |
dynadock PA3686U-1SET dynadock wireless |
dynadock PA3778U-1PRP dynadock V |
dynadock PA3927U-1PRP dynadock U3.0 |
dynadock PA5082U-1PRP dynadock V3.0 |
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using PKUnZip 2.04g or equivalent.
- Description
-
NR-123725-LS-1_R7.5_M2_DisplayLink_USB_Graphics_Software_for_Windows ===============================================================================
===============================================================================
DisplayLink Software Release: External Release Note
Software Package: DisplayLink Graphics
Product Version: 7.6.55102.0
Product Date: 25th April 2014
DisplayLink Core Software Version: 7.6.55049.0
DisplayLink Core Software Date: 22nd April 2014
DisplayLink DL-3xx0 / DL-5xx0 Firmware Version: 8.8.6.62033
DisplayLink DL-41xx Firmware Version: 8.8.6.62033
===============================================================================
===============================================================================
A. Introduction
===============
This is the R7.6 Product Release. It has been put through a full system test
and is suitable for deployment to end-users.
This is the last major DisplayLink software release to support Windows XP.
DisplayLink Software Release R7.6 delivers the following features:
- Support for DL-5500
- Disabled and Removed "Optimized for Video" from the DisplayLink UI
For further support and information about DisplayLink software, please visit
http://www.displaylink.com/support
A1. Important notes about DL-3xx0, DL-41xx and DL-5xx0 Firmware
======================================================
This software release contains an embedded firmware image.
DL-3xx0/DL-41xx/DL-5xx0 devices will be automatically upgraded with this
firmware upon connection.
B. Contents
===========
A. Introduction
A1. Important notes about DL-3xx0, DL-41xx and DL-5xx0 Firmware
B. Contents
C. New features
C1. Fixed issues since R7.5 M2 (7.5.54609.0)
D. How to Install and Use
E. Supported Operating Systems
F. PC Recommended Specifications
G. Language Support
H. Supported Hardware
I. Known Issues and Limitations
C. New features
===============
DisplayLink Software Release R7.6M0 delivers the following features:
- Support for DL-5500
- Disabled and Removed "Optimized for Video" from the DisplayLink UI
C1. Fixed issues since R7.5 M2 (7.5.54609.0)
--------------------------------------------
Monitor connected to DVI can show frozen screen on DL-3950 devices with
Displayport and DVI outputs after multiple DVI hotplugs (17128)
The hardware ID of monitor connected to DisplayLink device is branded
as "Default Monitor" on XP and Vista (16976)
Miracast stops working when DisplayLink driver is installed
on Dell Venue 8 Pro (16758)
Monitor connected to HDMI output does not show pixels if using same video
timings as monitor connected to VGA output (16703)
The last MAC address in the multicast filtering list is sometimes not applied
(17101)
On some systems, with high resolution in-build screens, monitors connected
to DisplayLink outputs can show slight corruption when resuming from suspend
(16200)
Add 2048x1152 and 1900x1440 modes when a 2560x1440 HDMI display is connected
(17209)
Installer compatibility check could sometimes incorrectly detect 3rd party USB
graphics software installed (17201)
Sometimes Displaylink monitor flickers when running DirectX application in full
screen (16260)
Desktop Windows Manager can crash occasionally when changing
window size (16963)
Some modes supported by monitor are not available to the user (16709)
D. How to Install and use
=========================
Please find detailed guidance and information about how to install and use this
software in the DisplayLink Software User Guide: http://kb.displaylink.com/298
Corporations can apply for a corporate install version at
www.displaylink.com/corporateinstall
For further support and information about DisplayLink software, please visit
http://www.displaylink.com/support
E. Supported Operating Systems
==============================
This release can be installed on the following operating systems:
- Windows XP SP2 (32-bit edition only)
- Windows XP SP3 (32-bit edition only)
- Windows Vista SP1 (32-bit and 64-bit editions)
- Windows Vista SP2 (32-bit and 64-bit editions)
- Windows 7 (32-bit and 64-bit editions)
- Windows 8 (32-bit and 64-bit editions)
- Windows 8.1 (32-bit and 64-bit editions)
- Windows 8.1 Update 2014 (32-bit and 64-bit editions)
- Windows Server 2008 (32-bit and 64-bit editions)
(This OS has received limited testing)
- Windows Server 2008 R2
(This OS has received limited testing)
Windows 2000 SP4 is supported by older versions of the DisplayLink software:
http://www.displaylink.com/downloads
Video: video is supported in extend mode with most popular video players on
Windows XP - Windows 8.1.
Installation on Windows Server 2008 R2 is enabled, but untested. End users may
try to use DisplayLink on server editions, but these are not supported
configurations.
F. PC Recommended Specifications
================================
Please find detailed information about the minimum and recommended system
specifications needed to run this software in the DisplayLink
Software User Guide: http://kb.displaylink.com/298
G. Language Support
===================
Please find the complete list of languages supported by this software in the
DisplayLink Software User Guide: http://kb.displaylink.com/298
H. Supported Hardware
=====================
Devices supported:
- DL-5500 / DL-5700 / DL-5900
- DL-41xx
- DL-3100 / DL-3500 / DL-3700 / DL-3900 / DL-3950
- DL115 / DL125 / DL165 / DL195
- DL120 / DL160
I. Known Issues and Limitations
===============================
System behaviour with DisplayLink attached screens has been well tested.
Testing covers plug/unplug, mode changes, playing video, hibernate,
sleep/standby, multiple users, different user rights, attached screen as
primary screen, attached screen as only screen, and other aspects.
Some use cases may exhibit minor issues, general troubleshooting
recommendations are:
- detach then reattach the DisplayLink device's USB cable
- change display settings using DL-GUI
- change display settings using WDP
- ensure you have the latest graphics drivers installed for your system GPU
For information about specific issues please see the DisplayLink support
knowledgebase: http://www.displaylink.com/support/knowledgebase.php
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.