Driver and Firmware for Wireless Speaker PA5147U-1SPB
- File: BlueSuite_2.5_W...
- Version: 2.5
- Posted Date: 2014-04-28
- Firmware Update Instructions
Prior to upgrading you will need a USB Data cable to transfer data from you PC USB port to the USB port on the back of the Bluetooth speaker. The USB power cable that came with your Bluetooth speaker will not work for this because it is only a USB power cable.
This update tool only works on computers running Windows 7 32 bit OS.- Download and unzip the file called BlueSuite_2.5_Win7.zip
- Right click on the extracted file called BlueSuite 2.5_Win7.exe and select "Run as administrator"
- If you are prompted to allow the following program to make changes to this computer verify the publisher as “Cambridge Silicon Radio Ltd.” and click Yes
- Select next
- Read the Software License Agreement then select “I Accept the License agreement”
- Select next
- Select next to accept the default installation location
- Select next to select default component list
- Select next to select the default start menu folder
- Select next to select Additional Tasks
These tasks should be check marked by default:
- “Install the SPI LPT device driver.
- “Set debug transport to LPT SPI”
- “DFU Tools Environment …”
- Select Install when ready to install
- Select Finish to “restart the computer now”
- After the computer reboots:
- Hold the power button down on the speaker for 30 seconds
- During this time the speaker will beep and shut off or come on then beep and shut off
- Release the power button on the speaker (after the power light has completed turned off)
- Press and hold the power button again while performing the following steps.
During the following steps you must continuously hold the power button down on the speaker.
- The speaker will power ON after a few seconds.
- The speaker will then power off again after about 20 seconds
- A beep should be heard from the speaker when it powers off this time.
- Connect a USB data cable between the speaker and PC.
- The computer will now start to install the device driver software
- When you receive the windows message that the “CSR BlueCore Bluetooth” “Device driver software installed correctly” you can release the power button
NOTE: If the “Device driver software installed correctly” does not appear after 1 minute you can release the power button and continue. In device manager you should see “CSR BlueCore Bluetooth” under the Universal Serial Bus Controllers if the device driver software installed correctly.
- Press the Windows start button
- Select All Programs
- Select CSR BlueSuite 2.5.0 folder
- Select DFUWizard
- Select next to Start the firmware upgrade process
- Select Universal Serial Bus (USB)
- Select next
- Select “Download a new version of the firmware, saving a copy of the current version first. Any previously saved version will be replaced. (Recommended”
- Browse to and select the file Toshiba TY-SP3(SH200)_V2.1.14_USA_BASS ON(+4dB).dfu
- Select next
- Select next when ready to upgrade
- When the upgrade has completed the message prompt will say Successful Upgrade
- Select Finish to complete the update process
- Your Bluetooth wireless speakers is now updated and you can disconnect the USB cable
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.