TOSHIBA System Driver
- File: os2014330a_tc00...
- Version: 1.00.0039
- Posted Date: 2014-07-25
- Release Date: 2014-07-22
- Other Versions
- Package
- WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
- Description
-
This is the TVALZ driver for Windows 8.1. This driver includes the Bluetooth ACPI, and TOSHIBA Hot Key drivers.
Driver Install Instructions
- Save the file to a convenient location like the Windows Desktop.
- Save all work in progress and close open applications.
- Click Install.
- Click Start when the TOSHIBA Archive Extractor dialog is displayed.
- Click Yes if a User Account Control Window is displayed.
- Click Yes when you see "This setup will perform an upgrade of 'TOSHIBA System Driver'. Do you want to continue?"
- Click Next when the "TOSHIBA System Driver - InstallShield Wizard" dialog is displayed.
- Click OK after confirming that "Automatically close and attempt to restart applications" has been selected.
- Click Finish after the installation completes.
Driver Version Verification
- Open Control Panel.
- Select Programs and Features.
- Verify that TOSHIBA System Driver version is 1.00.0039.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.