Bluetooth Stack for Windows by Toshiba

Package
WinZIP self-installing ZIP file. Can also be unZIPped using WinZip, PKUnZip or equivalent. Also supports silent installation. Click for silent/unattended installation instructions.
Description

This is a Bluetooth Stack for Windows by Toshiba update

Changes in this update

  1. This update fixes Security Vulnerabilities discussed in Toshiba Bluetooth Stack Security Update.

  2. Installation Instructions

    1. Download and save this file to a convenient location such as the Windows Desktop.
    2. Save all work in progress and close open applications.
    3. Double-click the downloaded file TC00636200a.exe to start the installation.
    4. Press the Start button at the Toshiba Archive Extractor window.
    5. Press Yes if a User Account Control message is displayed.
    6. If Bluetooth Stack for Windows by Toshiba v9.10.32(T) is applied successfully, the message below will be shown. Click Yes to restart the system.
Export Control and EULA
Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.