BIOS version 1.60 for Satellite P70/P75 (PSPLNx/PSPLPx)
- File: splnv160.exe
- Version: 1.60
- Posted Date: 2015-04-22
- Release Date: 2015-03-17
- Other Versions
-
Release Date: Version: 2014-06-20 1.50 2013-12-11 1.40 2013-10-08 1.10 2013-06-14 1.00
- Package
- WinRAR self-extracting ZIP file includes both Windows-based and diskette based BIOS update installation options. See the included documentation for details.
- Description
- For CD-ROM BIOS updates in Windows 8x models: (1) Shut down the system while pressing the SHIFT key to completely power off. (2) Power on while pressing F2 to enter the BIOS Setup menu. (3) From the Security tab and set the "Secure Boot" setting to "Disabled". (4) From the Advanced tab, enter "System Configuration" and set the Boot Mode to "CSM Boot" if the option is available. (5) Press F10 to save and exit. (6) Boot from the BIOS CD-ROM. (7) Type BIOS at the prompt then press Enter. (7) After the BIOS update has completed, restore the BIOS settings that were changed.
- Note: The BIOS Launcher "CD_ROM Installation" option may not automatically proceed to burn the CD-ROM in Windows 8. If this occurs navigate to the directory named after the BIOS filename in the root directory of the C-Drive (ex. C:\skgjv130), and manually burn the CD-ROM from the disc image (ISO) file.
- For CD-ROM BIOS updates in Windows 7 models: (1) Boot from the BIOS CD-ROM. (2) Type BIOS at the prompt then press Enter.
- For all updates: The BIOS update will force the computer to shut down or restart. Please make sure to save all work in progress before starting BIOS updates.
- Power on the computer if it is off.
- While the "TOSHIBA" logo is displayed, press the F2 function key to start BIOS Setup.
- Check the version of BIOS and press the F9 function key then Enter to load setup defaults.
- Press the F10 function key then Enter to save settings and exit. The computer will automatically reboot.
Release Notes
Change History
- Version 1.60 - 2015-03-17
- Fixed: NVIDIA graphics model Blue Screen of Death (BSOD) during a stress, sleep (S3/S4), and reboot test.
- Updated: Management Engine (ME) to 9.0_1.5M_9.0.31.1487.
- Added: Support for Windows 8.1.
- Updated: Intel ME firmware to ME9.0_1.5M_9.0.20.1447 for Windows 8.1.
- Updated: Intel CPU Microcode to M32306C3_00000016.
- Updated: GOP driver to V5.0.1032 and VBIOS 2177.
- Fixed: External monitor has LCD noise when the Power-on display is set to "External Display Device".
- Added: Support for the Chicony WB335 Bluetooth combo card.
- Fixed: Windows 8.1 RF LED issue when airplane mode is on.
- Updated: EC to version 1.30.
- Added: System shut-down process when unsupported 1.5V DDR3 RAM modules are installed. Only 1.35V DDR3L modules are supported.
- Updated: N14P-GS (80.07.A4.00.0A) and N14P-GV2 (80.28.28.00.22) VBIOS for new VRAM.
- Updated: Intel CPU microcode.
- Changed: Internal TV tuner controller (on supported models) from XHCI to EHCI.
- Added: Modification to support Windows 8.1.
- Fixed: Will not wake from Hibernation (S4) on systems with an external HDD, and the HDD password is set.
- Updated: Non-English string in the System Configuration Utility (SCU) Help Bar.
- EC Update - Fixed: Touch Screen does not work when the battery or AC Adapter are plugged in for the first time.
- Initial production BIOS for these models.
- Export Control and EULA
- Use of any software made available for download from this system constitutes your acceptance of the Export Control Terms and the terms in the Dynabook end-user license agreement both of which you can view before downloading any such software.